Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Part of the AutoORG® - mySAP PLM CADENAS integration are the following files:
sapcadenassrv.exe (executable program file) (Default: RFC-Library used)
Sapcadenassrvu.exe (Optional: RFC-Unicode Library used)
Sapcadenassrvnw.exe (Optional: NetWeaver Library used)
(One out of these files is used)
This is the central file both for the SAP MM integration and for the SAP PLM integration. You can find a detailed description under Section 3.3.8.10, “Integration file "sapcadenassrv.exe"”.
sapcadenassrv.ini (general configuration file)
This is the main configuration file from AutoORG® - mySAP PLM CADENAS integration.
A basic description is found in the configuration file itself.
Details are found in the installation manual "AutoORG® - mySAP PLM CADENAS Integration" of the CIDEON Software GmbH.
If you have any questions please contact the CADENAS Consulting Team.
saplogon.ini (primary configuration file for the connect to the SAP system)
saprfc.ini (secondary configuration file for the connect to the SAP system - all settings are also possible via saplogon.ini)
saptrans.ini (configuration file for calling up any SAP transaction)