powered by CADENAS

Manual

Manual

5.15.2.6. Background information

Fig. „Diagram: Workflow - Catalog Update “ shows the procedure at an catalog update.

  1. PARTadmin -> Catalog update

    Comparison of the catalog date

  2. Comparison of the projects

    Project path, Project name and Standard number are checked for changes.

    • If projects have been cancelled, this is identified by the version number of the old project.

    • If a newer version has been added, this is identified by the version number of the old project and a new project is created.

    • If it is not possible to find a relation to an existing project, a new project is created.

The points 1 and 2 are basically performed, even if there is no ERP integration.

  1. Comparison of the project lines (especially this point is part of Section 5.15.2, “ Catalog update with ERP integration - Update manager ”)

    "Additional project lines" (see diagram) cannot have a link in the LinkDB. No further checking is processed.

    At all project lines, which have a link in the LinkDB, an exact checking of changes (project, table, geometry) can be processed.

    Furthermore the values in the LinkDB columns "ACTIVE_STATE" and "REQUESTED_STATE" are adjusted.

Diagram: Workflow - Catalog UpdateCatalog updateDiagram

Diagram: Workflow - Catalog Update