5.1.4.2.4.
New installation of parts using an ERP Interface
PARTsolutions user wants to use a part,
of which he still does not have an ERP number.
The interface opens an ERP mask, in which
data for the corresponding part are already inserted.
The user fills in the
missing data, like for instance material (geometric data will be
automatically transferred)
The interface applies
this part to the ERP system with a new ERP number and the whole
dataset is transferred to the LinkDB.
Advantage: Complete
integration of PARTsolutions in the ERP system when creating a new
part; new parts can be applied from PARTsolutions and are
immediately available in PARTsolutions, by the automatic creation
(from PARTsolutions) part redundancy will be prevented.
Required module ERPsolutions + (e.g.) SAP
MM Gateway or an individually programmed Gateway.
Note
Manual creation of parts
without Gateway using the modules PARTdataManager and
PARTlinkManager is always possible.