You can use SSL encryption for all requests to the PARTapplicationServer [17].
Self signed or official[18] certificates can be used.
In the following the creation and the import of a self signed certificate is described:
Create certificate on the AppServer
In PARTadmin, select the category AppServer Service.
Activate the checkboxes for HTTPS-Port and/or SSL-Service-Port. Normally the others are deactivated. That means, unencrypted access to the server is not possible.
The dialog box Generate certificate... is opened.
Alternate Names: Both DNS names and IP addresses can be allowed. At the desired alternate names, activate the checkbox.
By default, a certificate is issued to the CommonName. If, for example, several websites are hosted, only one certificate is sufficient when using Alternate Names. The client will check whether the used hostname corresponds to one of the alternate names.
Protect key with standard password:
Import certificate on the client
Activate the checkbox Use SSL.
-> HTTP port and Service port are deactivated and HTTPS-Port and SSL-Service-Port are activated.
Tunnel services via web sockets (optionally):
You can use this option, if you want to bind only one port or if you want to connect via HTTP proxy (if websockets are possible).
When using this option the input field for SSL-Service-Port grayed out.
Little testing if everything is working properly: Make sure that Use SSL is activated. Click on . If the certificate is properly stored on the client, the server state is displayed, otherwise an error message is displayed.