powered by CADENAS

Manual

Manual

4.5.11.  AppServer Service: Authentication - Assign rights - Rights

In PARTadmin under AppServer Service you can find the setting options concerning Authentication, Assign rights and Rights. Also important is to use HTTPS / SSL for the Port configuration (see below).

  • Authentication tabbed page: On subpage Mechanisms+Paths there is defined with which method and which condition authentication may happen.

    Under Prefix "/webapps" there is defined, that autologin is used, when coming from Web Browsers embedded in PARTsolutions or PARTsolutions applications.

    "Authentication" tabbed page

    "Authentication" tabbed page

    [Note] Note

    In order to view all Users/groups, activate the option Active and click on Reload.

  • Assign rights tabbed page: Listing of assigned users and groups or all existing users and groups in all trusted Domains/Forests

    By default, a logged in user can view, control and delete his own pipelines.

    "Assign rights" tabbed page (only assigned)

    "Assign rights" tabbed page (only assigned)

    If you want that a certain user has extended rights, proceed as follows:

    1. Under Known users/groups, select the option all existing.

      -> All User/Groups are listed.

      "Assign rights" tabbed page (all existing)

      "Assign rights" tabbed page (all existing)

    2. Under Users/groups, select the desired user.

    3. On the right, under Profile, activate desired.

      [Note] Note

      Should there be no fitting default profile, you can define your own on tabbed page Rights.

  • Rights tabbed page

    Here you can add, remove, edit and copy Profiles and/or Rights, if needed.

    "Rights" tabbed page

    "Rights" tabbed page

Use HTTPS / SSL

  1. Use HTTPS and activate SSL (HTTP authentication is cleartext).

    Under category AppServer Service, on tabbed page Port configuration, activate the two checkboxes HTTPS-Port and SSL-Service-Port. A description on how to create a self signed certificate can be found under Section 4.5.7.3, “SSL encryption ”.

  2. Under category AppServer client, activate the option Use SSL and import respective certificate from server. See Section 4.5.7.3, “SSL encryption ”.