Pay
attention that no administration modules like PARTlinkManager and PARTadmin are installed on user
clients or restrict access via Windows authorization rights!
PARTadmin started without
administration rights
In some categories the
authorization rights are mandatory.
Note
Accessing files under
$CADENAS_USER is possible without administrative
authorization rights.
Thus language
settings can be performed without
administrative authorization rights.
Missing rights are identified by
the lock icon.
If the information symbol
is shown in the toolbar, this means
that PARTadmin was not
started in administrative mode. By clicking on the icon,
PARTadmin
is restarted - this time with Admin rights.
Note
The icon is only displayed
when the UAC-Modus is activated.