powered by CADENAS

Manual

Manual

5.5.1.4. "Active licenses" tabbed page

On the Active licenses tabbed page you receive detailed information on all active licenses.

At first select one of these two options:

  • Local

    The Nodelocked license products of the respective locale client are displayed.

  • On license server

    The Floating license products are displayed with the additional information, by which computers these are currently used.

    [Note] Note

    This information may be interesting, when the user did not get a license at the moment because there were no free licenses available anymore.

    [Note] Note

    Only FLM licenses are displayed (no Dynamic Nodelocked).

There are two product groups:

  • Base products

    Base products have to be reserved at the start of a program / an interface. (They are so to say the "base license".)

    Only one base product can be reserved at the same time (at floating).

  • Addons

    Addons can be reserved in addition to all modules. They don't have to be reserved at startup.

The column When to pull? shows, whether the product is reserved On startup or On demand.

The column Status shows, whether the product is In use or Not in use.

The column Trigger shows, which license key has been trigger for the product reservation.

Base products and Addons

Base products and Addons

Base products and Addons have the following subitems:

  • Modules

    All modules and interfaces are listed, which can be used with the respective license product.

  • Hosts

    ... shows the Mac address of the host

  • Features

    ... shows the single license keys, which are contained in the respective license product.

    The column Status shows, whether the key is In use or Not in use.

    The column Trigger shows via Yes/No, whether the key has been trigger for the product reservation.

  • Details

    ... shows customer name, license type, issue date and number of products.