powered by CADENAS

Manual

Manual

2.2.4.5.3. Export standard attributes in several languages

Per default, most CAD systems have only one export language set for the standard attributes. If more than one language is to be exported simultaneously, then simply add the respective keys.

A foursome block must be applied for each language:

Orientate yourself to the existing default block when applying a new block.

When applying the new keys you must make the last digit high, or take an unused one (Attr_Content_00 -> Attr_Content_01)

Assembly of a section:

  • Attr_Content_xx

  • Attr_Section_xx

  • Attr_CopyFrom_xx

  • Attr_Prefix_xx

With both keys "Attr_CopyFrom_xx" and "Attr_Prefix_xx", you determine that the PARTsolutions standard attributes are to be exported to the CAD system with the indicated prefix in the defined language.

Example:

Attr_CopyFrom_01=default
Attr_Prefix_01=CNS_

Attr_CopyFrom_01=italian
Attr_Prefix_01=CNS_ITA_

In this way you can export the standard attributes in as many language versions - with the respective prefix - as you wish.

[Note] Note

If there is no translation for an attribute in the indicated language, no attribute will be exported (not even from the $CADENAS_LANGUAGE language).

Insert key: The figure is just an example. For each CAD system the specific system key in the "Attr_Section" key must be used. This key is already inserted and may not be changed!

Insert key: The figure is just an example. For each CAD system the specific system key in the "Attr_Section" key must be used. This key is already inserted and may not be changed!