powered by CADENAS

Manual

Manual

2.2.8.7.  Block [NoSection]

For connection elements such as screws, nuts, rings, pins, etc. the cutting in the 2D view may be excluded.

In image 1 below you can see that with activation of the respective classification attribute only the plate is cut and not the screw itself.

Image 1: Screw not cut

Image 1: Screw not cut

Image 2: Screw cut

Image 2: Screw cut

For desired projects, in PARTproject under Edit project -> General -> Classification > Attributes (CNS), the feature CNS_NOSECTION is set on 1. See Section 7.13, “ Add projects to classification ” in eCATALOGsolutions Manual.

[Note] Note

In exceptional cases, Consulting can step in via configuration file and so declare certain directories/projects in this way.

Local changes in the project file are not target-aimed, because these will get lost at next catalog update. Changes should be performed centrally during modelling process.