Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If in an update version a directory, project or certain characteristic is missing, then it can be the case that LinkDB links have no target.
As soon as a certain characteristic is selected in the index tree, you can recognize on the right side, in the section Line mapping as well that there is no assignment:
A missing automatic assignment of a project does not necessarily mean, that it does not exist; it could be that only the name has been changed.
For editing of assignments you have two options:
You can confirm the missing assignment now in the section Line mapping in the column New dataset via click on the green checkmark .
Now there are two further cases:
A new line assignment shall be made in the same project.
-> Hereto change the line selection in the table and confirm with the command Approve assignment.
A new line assignment shall be made in another project.
By clicking on the button Search project the dialog box Search opens on the tabbed page Search.
Perform a text or variable search.
By double-clicking on one of the search results the desired part is assigned.
Alternatively you can switch to the Choose tabbed page and there browse to the desired part/project. Then you can load the project via double-click into the column New dataset. Now select the desired characteristic.
Regardless of the chosen variant now finally confirm the new assignment by clicking on the green checkmark Approve assignment.