powered by CADENAS

Manual

Manual

4.21.1.  Load additional scripts - erpcustom.cfg -> Block [LOAD]

Optionally, activate additional functionality for ERP.

PARTadmin -> erpcustom.cfg -> LOAD

PARTadmin -> erpcustom.cfg -> LOAD

PARTdataManager toolbar "LinkDatabase"

PARTdataManager toolbar "LinkDatabase"

 
1=$CADENAS_SETUP/scripts/erp/
erp_displaymat.vbb
Display material master in SAP
 
2=$CADENAS_SETUP/scripts/erp/
erp_searchmat.vbb
Search SAP material number in SAP
 
3=$CADENAS_SETUP/scripts/erp/
erp_mapping.vbb
Required for the SAP-MM connection
 
4=$CADENAS_SETUP/scripts/erp/
sap_base.vbb
Required for the SAP-MM connection
 
5=$CADENAS_SETUP/scripts/erp/
erp_asmtables.vbb
 
6=$CADENAS_SETUP/scripts/erp/
erp_psol_mm_vars.vbb

Add dataset to link database (variant) (PARTdataManager)

(If the key does not exist please add it with incremented number.)

Also see Section 4.7, “ERP toolbar and menu ” -> item "Add dataset to link database (variant)".

In order to open the SAP material master the following key is required in addition.

  • KEY 4=$CADENAS_SETUP/scripts/erp/erp_sap_mm.vbs

    Also see Customizing der PARTsolutions-ERP-Schnittstelle.

7=$CADENAS_SETUP/scripts/erp/
erp_dbedit.vbb

Edit/delete dataset: Create new material number, SQL query (PARTdataManager)

 
erp_export_ts=$CADENAS_SETUP/scripts/
erp/erp_export_ts.vbb

Directly after clicking the export button an ERP_PDM_NUMBER is automatically created and the new line is saved in the link database.

The entry is immediately visible in PARTdataManager.

Via $CADENAS_SETUP/erpcustom.cfg -> Block [dialogOnExport] you can control whether the process shall be silent without dialog or with dialog in order to be able to select the desired material.

See Section 4.11.2, “ erpcustom.cfg -> Block [dialogOnExport] - Automatic generation of ERP number: Export dialog for material and other fields yes/no ”.

show_dbdata=$CADENAS_SETUP/scripts/
erp/show_dbdata.vbb
Shows the ERP columns among each other in a separate info dialog (clearer depiction)