Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
With the help of the function, old catalog versions that are no longer needed, can be removed from the index tree.
If catalogs are renewed through updates in the course of time, the existing catalog data are not deleted, but rather receive a time stamp add-on in their file attachment, which stands for the respective version of the catalog (see image below).
The higher the number, the newer the catalog status.
You can call Cleanup versions either via Commands or via the context menu of the catalog.
In the following the single functions are explained.
Concerns e.g. PARTdataManager -> "History" tabbed page (see next figure, compare Section 1.3.3.1.5, “Check project changes in detail (after the installation) ”) |