Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the
configuration file material_assign.cfg
you can
define, which materials shall be displayed in PARTdataManager, in the
dialog box new ident-no..
When exporting to the CAD system the PARTsolutions material is mapped onto the CAD system material, so that the physical properties can be calculated in the CAD.
Information on the transfer of the material attribute to the CAD system is found under Section 2.2.5, “Material mapping ”.
Information on the integration of the material into the file name is found under Section 2.2.2.2, “File name: set generation options ("FileName" key) ”. Per default an available material information is overtaken into the file name.