Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The accuracy search can be configured using the following settings:
If the accuracy settings of the Pro/E part template differs from the accuracy of the part in PARTsolutions, it is possible that the part cannot be created in Pro/E.
Then the error message "Part could not be created" shows up.
Using the "AdjustAccuracyOnFail" setting, the geometry export can be configured in such a way that an automatic search for the appropriate accuracy settings of the part is conducted. If this setting is activated (AdjustAccuracyOnFail=1), an accuracy search is carried out if necessary. This concerns the calculation of accuracy of the sketches as well as the accuracy data of the entire part.
Important | |
---|---|
With the activated accuracy search, the accuracy of a part may differ from the accuracy of the Pro/E part template. The actual accuracy must thus be checked manually. |