Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.3.8.3.
Attribute mapping in
SolidWorks
2.3.8.3.2. Block
[CadDocumentAttributes] - Transfer custom attributes
|
|
---|---|
Prev | Next |
Attributes which are declared in the block CadDocumentAttributes are displayed in SolidWorks in the dialog box File information -> Tabbed page Custom as extra attributes behind the standard attributes.
In order to define the display value of the extra attributes for SolidWorks, do the following:
Enter the desired value into the input fields of "Description" and "PartNo".
ARTICLENO=?_ATTR("NB") BOMINFO=?_ATTR("LINA")
You can change the attributes itself or the text outside the angle brackets.
Text-<ATTR(NN)>-Text-<ATTR(NT)>-Text
- > For all exported parts you can now see the mapped attributes under File information -> tabbed page User-defined.
You may set as many keys as you like.
The following figure shows the result in SolidWorks in the "File information" window on the "User-defined" tabbed page.