powered by CADENAS

Manual

Manual

4.8.8. Determine column color by indicator in ERP column (very special) / plinkgroups.cfg -> Block [<Role_name>] -> Key "COLORNUMBERTREE"

When using the key "COLORNUMBERTREE" add a column "COLOR_COLUMN" (type "Integer") in the ERP table.

This column can be filled with numbers from '0' to '9'.

Then, according to the condition under the key "COLORCONDITIONTREE0" to "COLORCONDITIONTREE 9" the respective color is shown.

Default value:

COLORNUMBERTREE=MIN(ERPTABLE.COLOR_COLUMN) 

Because of the "MIN" the lowest color number has the highest priority, if there are different values in "COLOR_COLUMN" for the respective project or directory.