Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Material(is3dpart)=?context.TranslateStringInGlobalOptionArrayDef("MATMAP","",_FORMAT_0 ("<CLASSPROP(cns,CNSPHYPROP,CNSMAT)>").value(),_FORMAT_0("<CLASSPROP (cns,CNSPHYPROP,CNSMAT)>").value())
By default, the value of the key Material(is3dpart) is acquired with a complex VBS expression.
The "TranslateStringInGlobalOptionArrayDef" function takes the string from its third parameter and attempts to look it up in the [MatMap] block. If this is successful, the mapped value is transferred to NX. The fourth parameter is the default value. If the searched material name cannot be found in the [MatMap] block, this default value is returned instead. With the default value set to be the same as the input value, the latter is transferred to NX unchanged if the MatMap lookup fails. (#41677)
Hinweis | |
---|---|
The untranslated name of the material is transferred; in other words it will be the same for all languages. |
Valid names
are normally located in C:\Program Files\Siemens\NX
8.0\UGII\materials\phys_material.dat
. E.g.: Sodium_Liquid,
Aluminum_6061 Alternative examples:
Zurück | Nach oben | Weiter |
2.3.5.1.2. Key "FileName" | Zum Anfang | 2.3.5.1.4. Keys "feature_group_xx" |