Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The jdbc.cfg is for the database connection data, i.e. Server, Database, in particular the driver class and the URL for the jdbc driver to establish a connection to the database.
This file is organized in DSNs like the following:
# [PLINKDB] # #IP-adress or server name # Server= # #Database name # ServerDB= # #the jdbc driver class # DriverClass=com.sap.dbtech.jdbc.DriverSapDB # #the complete URL for the jdbc driver # URL=jdbc:sapdb://catia2.cadenas/PLINKDB #Examples for different databases: -------------------------------- #MSSQL with JTDS #[PLINKDB_MSSQLJDBC] #Server=136.230.230.214 #ServerDB=DB-test #DriverClass=net.sourceforge.jtds.jdbc.Driver #URL=jdbc:jtds:sqlserver://136.230.230.214:1433/PLINKDB #Oracle: #[PLINKDB_ORACLEJDBC] #DriverClass=oracle.jdbc.driver.OracleDriver #URL=jdbc:oracle:thin:@servername:1521:PLINKDB #SAP-DB: #[PLINKDB_SAPDBJDBC] #DriverClass=com.sap.dbtech.jdbc.DriverSapDB #URL=jdbc:sapdb://servername/PLINKDB #MySQL: #[PLINKDB_MYSQLJDBC] #DriverClass=com.mysql.jdbc.Driver #URL=jdbc:mysql://servername:3306/PLINKDB #Derby (local) (Experimental!): #[PLINKDB_DERBYJDBC] #DriverClass=org.apache.derby.jdbc.EmbeddedDriver #URL=jdbc:derby:C:\data\derby\plinkdb #Derby (net) (Experimental!): #[PLINKDB_DERBYJDBC] #DriverClass=org.apache.derby.jdbc.ClientDriver #URL=jdbc:derby://localhost:1527/plinkdb #Firebird (Experimental!): #[PLINKDB_FIREBIRDJDBC] #DriverClass=org.firebirdsql.jdbc.FBDriver #URL=jdbc:firebirdsql:host[/port]:/path/to/db.fdb #example: jdbc:firebirdsql:ora10:/Dokumente und Einstellungen/Administrator/Desktop/firebird /data/PLINKDB.FDB#Path is relative to server without drive letter. Data has to be in the same folder of the service executable. #SQ-Lite (pldbdemo) [PLDBDEMO_SQLITEJDBC] #:VALS_S #:HELP;default;IP-adress or server name, on which the database is installed Server=localhost #:VALS_S #:HELP;default;The instance name of the database. Oracle: SID ServerDB=pldbdemo #:VALS_S #:HELP;default;The jdbc driver class. DriverClass=SQLite.JDBCDriver #:VALS_S #:HELP;default;The complete URL for the jdbc driver. Url=jdbc:sqlite:/$CADENAS_USER/sqlite/pldbdemo.db3
For example, in the case of a PLDBDEMO installation the name PDBDEMO_SQLITEJDBC is used for database connection. This description should also be set in the PARTlinkManager under Extras --> ERP-Umgebung konfigurieren --> tab Datenbank.