powered by CADENAS

Manual

Manual

2.3.2.7.1.21. Key "COMMAND_SHOW_PSOLDRWPartConnect"

Drawing Toolbar - Activate the command that should be loaded at startup and set the value on "Yes". If a key is disabled the code and command will not be available in CATIA.

Verschraubungen

COMMAND_SHOW_PSOLDRWPartConnect

Connections section in PARTdataManager is opened.

[Hinweis] Hinweis

In order for the commands to be displayed in the PARTsolutions toolbar, you have to edit the respective keys starting with "MN_" in addition.