Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Settings for starting the application server.
[INIT] ;Indicates if threads should be used while application server starts (as of 1.7) UseThreadsForStartup=true ;Defines the editable parts amount of threads (as of 1.6) NumberEditablePartServiceThreads=2 ;Defines the amount of threads for the tree (as of 1.6) NumberIndexItemServiceThreads=4 ;Defines the amount of threads for the table (as of 1.6) NumberPartListServiceThreads=4 ;Defines the amount of threads for the search (as of 1.6) NumberSearchServiceThreads=3 ;Sets the factor to calcualte the minimal free memory depending on the total ;memory (as of 1.7) FreeMemoryFactor=0.1 ;Sets the level of index items which should be loaded at startup (as of 1.7) IndexItemLevel2Load=0 ;Sets the allowed start up catalogs (as of 1.7) AllowedStartUpCatalogs=.* ;Sets the hidden start up catalogs (as of 1.7) HiddenStartUpCatalogs=.*_qa|.*_dev ;Sets the allowed start up class systems (as of 1.7) AllowedStartUpClassSystems=class_catalog_classification|class_countryconnection ;Sets the hidden start up class systems (as of 1.7) HiddenStartUpClassSystems=
Zurück | Nach oben | Weiter |
4.7. Configuration file | Zum Anfang | 4.7.2. CATALOG |