powered by CADENAS

Manual

Manual

1.1.6.10.1.4. Special settings in partsolu.cfg
  • sortToolbars

    With the help of the key sortToolbars under $CADENAS_DEFAULT_USER -> block [TWEAKMENU] the position of the toolbars is saved. When restarting the application the set positions are recovered.

    Example:

    toolbarOrderTop=Standard,Assembly,Details,Export,\n,Views,LinkDatabase,Addsap,IndexTree

    The value of the config key will be set to 0 when the application is closed.

  • Key PARTdataManager_Mode (or PARTproject_Mode)

    The key saves the mode (Beginner / Professional) which is used when opening the application. Under Extras menu -> Mode auswählen you can switch anytime.

  • Add further applications to be controlled by tweak configs

    If you want to add a new application, which should be controlled by the tweakmenu you must insert the name of the application as value of the key processedApps in the $CADENAS_USER/partsolu.cfg. Of course you have to create the two configs, which are described above. Copy the content of menustructure_PARTdataManager.cfg and menuvisibility_PARTdataManager.cfg to get a quick start.