powered by CADENAS

Manual

Manual

1.8.2.1. How can I select a CAD format? | How can I define the transfer mode into the CAD system? (Supplier portals)

In the following you can find a description how to specify formats and how to determine the transfer mode to the CAD.

  1. On the right side under Download CAD models, click on Edit CAD formats .

    -> The dialog area Actions is displayed.

  2. Click on Add CAD formats.

    -> The settings area for Generation type and Format selection opens.

    Generation type und Format selection The following formats for 3D CAD models and 2D CAD models are available (license dependent): ADEM | Alibre Design | Architectural Desktop | AutoCAD | BMP (2D View) | BMP (3D View) | CADCEUS | CADISON | CADdy | CadKey | Cadra | CATIA | Cimatron | CoCreate Modeling | Creo Elements/Direct Modeling | Creo Elements/Pro | Creo Parametric | DWF | DWG | DXF | Geomagic Design | Helix | HiCAD | Ideas | IGES | IntelliCAD | Inventor | IRONCAD | JPEG (2D View) | JPEG (3D View) | KeyCreator | KOMPAS | LogoCAD | Mastercam | Mechanical Desktop | Medusa | MegaCAD | MI | Microstation | NX | One Space Modeling | Parasolid | PDF 3D | PDF Datasheet | Pro/ENGINEER Wildfire | PRO-Desktop | SAT | Solid Designer | Solid Edge | SolidThinking | SolidWorks | SpaceClaim | STEP | STL | SVG | thinkdesign | TIFF (2D View) | TopSolid | TurboCAD | Unigraphics | Vectorworks | VDI | VISI | VX

    Generation type und Format selection [9]

  3. First determine the desired generation type. Click into the desired option field.

    Select Generation type

    Select Generation type

    [Note] Note

    You can define own formats for each generation type.

    • CAD models to download

      After generation, the CAD models are available in the Download CAD models area.

    • Direct integration into CAD system

      The direct integration (PART2cad) simplifies the download of the CAD models. These are then quickly and directly loaded into the CAD system. The temporary saving of data is thus omitted.

      [Note] Note

      Only one format selection is possible in this mode.

    • CAD models sent per e-mail

      The CAD models are sent per e-mail immediately after generation.

    [Note] Note

    In the Format selection area , the formats possible for the selected mode are displayed.

  4. Select a format or several formats. By holding down the CTRL key, you can make multiple selections.

    [Note] Note

    Max. 10 formats (in total for all generation types) is possible.

  5. Click on Save.

    -> The view returns to the dialog area Selected formats.

    In the dialog area Selected formats you can see your current selection.

  6. Confirm your entries with Save.

    [Note] Note

    You can now repeat the format selection for another generation mode if desired. Go back to Add CAD formats.

    -> The current format selection is shown.



[9] The following formats for 3D CAD models and 2D CAD models are available (license dependent): ADEM | Alibre Design | Architectural Desktop | AutoCAD | BMP (2D View) | BMP (3D View) | CADCEUS | CADISON | CADdy | CadKey | Cadra | CATIA | Cimatron | CoCreate Modeling | Creo Elements/Direct Modeling | Creo Elements/Pro | Creo Parametric | DWF | DWG | DXF | Geomagic Design | Helix | HiCAD | Ideas | IGES | IntelliCAD | Inventor | IRONCAD | JPEG (2D View) | JPEG (3D View) | KeyCreator | KOMPAS | LogoCAD | Mastercam | Mechanical Desktop | Medusa | MegaCAD | MI | Microstation | NX | One Space Modeling | Parasolid | PDF 3D | PDF Datasheet | Pro/ENGINEER Wildfire | PRO-Desktop | SAT | Solid Designer | Solid Edge | SolidThinking | SolidWorks | SpaceClaim | STEP | STL | SVG | thinkdesign | TIFF (2D View) | TopSolid | TurboCAD | Unigraphics | Vectorworks | VDI | VISI | VX