Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
For a catalog update a simple check for possible assignment problems in the LinkDB can be performed.
Immediately when starting the update the following message is displayed.
If you want to perform the check, click on .
If no problems are detected, the installation is executed without any further notes.
If problems are detected, the dialog box CIP Installation appears. On the tabbed pages ERP Status and PLM Status, the single projects are listed with their status, so that you can decide, whether you want to perform the installation or not.
Dialog box "CIP Installation" with tabbed pages "ERP Status": Here exemplified, the different status such as "to check", "successful" or "not mapped" are displayed.
If yes, then click on the button .
Note | |
---|---|
With the help of the Update manager you can later go through the problematic projects and perform assignments. |
When clicking on the installation is running through. Finally the note on allocation problems is displayed.
Open the Update manager by clicking on the link or open it later in the PARTlinkManager under Extras menu -> Update manager.
On the left, in the directory structure, you can select single projects and lines. On the right you can see the current mapping. When clicking on the respective icon you can approve or revoke assignments.
Details on the Update manager can be found under Section 4.16.3, “Catalog update with ERP integration - Fix mapping problems with the Update manager ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
More details on the catalog update with ERP integration can be found under Section 4.16, “ Catalog update with ERP integration ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
Note | |
---|---|
As of V10, mapping information can be created from one to the next catalog version by the catalog modeling. That means, then mapping has not to be performed on the customer side at each update. Details on this can be found under Section 8.9, “ Add ERP-Mapping... / Edit ERP-Mapping... ” in eCATALOGsolutions Manual. |