powered by CADENAS

Manual

Manual

3.2.1.6. Select release directory / Set up new share

You can either use a current release or set up a new one

  • Use existing release:

    Click on Choose share and determine the server directory.

    Set up release

    Set up release

  • Set up new share :

    Click on the button Create new share.

    [Note] Note

    Set up shares only via installation program, NOT manually in the file system!

    --> A dialog for defining a share directory opens up

    Determine share directory

    Determine share directory

    Via the Browse ... button, define the Share directory and under Name of the share enter the desired name.

    [Note] Note

    Shares can only be created on the installation computer itself. Otherwise you will receive the error message to the right.

    Share could not be created.

    Share could not be created.

    When creating a share successfully, you will receive a confirmation message.

--> The share path has now been entered.

Enter share path

Enter share path

If you want to use the same share for both the PARTsolutions program data, the catalog data and the setup directory, you are now finished.

Otherwise, by activating the respective checkbox, you can set up your own shares for $CADENAS_DATA and $CADENAS_SETUP.