powered by CADENAS

Manual

Manual

3.10.  Automatic Classification of standardized Parts

When a new release CIP is generated via PARTproject also a scanner is running during this process in order to identify and classify all kind of standardized parts. Explicitly all NNs and NTs were checked whether they contain one of the below listed keywords followed by a number like “123”, etc.:

3-digit Keywords

DIN, ISO, ANSI B, NF E, VDI, UNI, NAS, NASM, BSI, ASNA, JIS, CSN, STN, GOST, JB/T, NIHS

2-digit Keywords

EN, SN, LN, AN, SN, BS, IS, KS, GB, PN, GB, MS, VG

Especially within the 2-digit keywords there is unfortunately a high rate of mistakes and wrong classifications, because e.g. „Rohrbogen 90°“ is recognized as a EN 90 (an "Euro Standard”). Wrong classifications like this can be sorted out by inserting a „NO“ into the filed Similar to standard parts (optional) in PARTproject tab General -> Similar to standard parts (optional). If a catalog has wrong classifications, it must be checked from time to time by the responsible Project Manager.