Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Via Export files in batch run you can create preview images used within the program for the directory structure.
In Part selection a preview image is located for each catalog, directory and project level.
The preview image for the catalog can be created externally and then imported. See Section 7.7.2.1.14.3.1.3, “Alternative: Create preview images externally and then import”.
For the preview images of parts, you also have an automatic variant available. Via the Export files in batch run command, the preview images can be created in the batch run. See Section 7.7.2.1.14.3.1.2, “Preferences”.
The function is available on project and directory level both in PARTdataManager [7], as well as in PARTproject:
[7] Only in Developer mode. Detailed information concerning the mode settings can be found under Section 1.1.6.6.2.3.1, “ Key "IsAdmin" - User mode ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.