powered by CADENAS

Manual

Manual

8.4.1.2.1.  Mandatory parameters

Each dimensioning must contain the following parameters:

  • ID

    The ID is automatically set.

  • Type

    When creating a new dimensioning at first a selection dialog box for the type definition appears. The type is displayed here.

    If it makes sense you may change the type via list field selection.

    [Note] Note

    The parameter fields are not updated until you have clicked Save changes .

  • Views

    At the desired 2D views, where the dimensioning shall be displayed, activate the checkbox.

  • Start point and End point

    1. In the 3D view, click on the desired connection point.

      -> This is marked in red now.

    2. Click into the input field of the point.

    3. Enter the name of the point via Ctrl+V from the clipboard into the input field.

      Example: Enter start point

      Example: Enter start point

  • Position (Distance dimension to the reference line)

    You can reference to the Bounding Box or the element:

    • BBOX

    • ELEMENT

    Examples:

    Dimensioning above the Bounding Box

    BBOX: 25

    BBOX: 25

    Dimensioning below the Bounding Box

    BBOX: -25

    BBOX: -25

    Dimensioning below the element

    ELEMENT: -15

    ELEMENT: -15

    Alternatively you can also use PARTdesigner-Expressions (see Section 7.8, “Functions - PARTdesigner-Expressions ”).

    15*RZ500@D/20