powered by CADENAS

Manual

Manual

6.3.4.1.1. Select *.3db object
  1. Run PARTdesigner within PARTproject.

  2. In PARTdesigner call up the desired Geometry (*.3db).

  3. Click the button 2D derivation .

    -> The same-named dialog box opens.

  4. Select the desired view type Front, Back, Right, etc. In the example Front is displayed.

  5. Reduce the 2D view so that you can see the History pane located behind it.

  6. Right-click on the context menu of plane XY (Sketch 1 was created there).

  7. Click on New 2D drawing.

    [Note] Note

    With PARTdesigner dimensioning views can be created and stored with a special name as 2-D sketches. Then they are available in PARTdataManager.

    -> The same-named context menu appears.

  8. Select an entry under View in the pull-down menu. Either a standard view corresponding to the chosen 2-D selection. (in this case the Description is automatically applied) or "USER" in order to insert a user-defined description.

    In the following figures USER has been taken.

  9. At content choose the option Accept current 2D derivation and confirm with OK.

    --> The view changes to 2D Sketcher.