powered by CADENAS

Manual

Manual

18.2.2.2.2.1.  Scale, position sketch elements in 2D view

Scale sketch elements:

  1. Activate the Edit mode:

    • Click into the view area with the right mouse button.

      In the context menu activate the Edit mode.

    • Or click on the respective button in the toolbar alternatively.

  2. Click into the sketch element.

    -> The red frame with the finger shows up in the right bottom corner.

Edit mode activateEdit modeactivate

Edit mode activate

  1. Deactivated:

    -> The display either changes continuously or progressively in set scales. See "No scale" in the next point.

Scale - 1: 10

Scale - 1: 10

No scale

No scale

No scale

  • Option No scale deactivated (scale used):

    Within the given frame the most fitting scale is used. The scale is displayed in the title (possibly only visible after enlargement).[70]

    Scale 1:10

    Scale 1:10

    Scale 1:10

    Scale 1:10

    Scale 1:5

    Scale 1:5

  • Option No scale activated:

    Within the given frame the entire available space is used. (Usually the derivations then increase in size.)



[70] The possible scales are defined administratively in the configuration file. See Section 1.1.6.7.1, “ 2dscales.cfg - Use scale for 2D view ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.