powered by CADENAS

Manual

Manual

8.6.6.1. Value take-over from the Measure dialog window

The Transfer button can be used for classifying native parts.

Do the following:

  1. Open a native part in the PARTdataManager.

  2. With Table --> Edit call up the Create tables window.

    Assign a classification to the native part (for example, under eClass 5.1).

    Classification allocated

    Classification allocated

  3. Under Attributes (classification) via the Search ... button, open the Class variables window.

  4. Select a class attribute.

    Cursor in "Value" field

    Cursor in "Value" field

  5. Set cursor on Value field.

  6. Click on Measure.

    --> The Measure dialog window is opened.

    2 parallel areas marked

    2 parallel areas marked

    In the 3D window, mark the desired areas, lines, points, etc.

    Click on Transfer.

    Detailed information on the measurement dialog can be found under Section 7.5.2.9, “ Measurement of 3D parts ”.

    ABS = 5.000 transferred

    ABS = 5.000 transferred

  7. --> The value is assigned to the currently measured class attribute.

    The value from the measurement dialog has been assigned

    The value from the measurement dialog has been assigned