powered by CADENAS

Manual

Manual

6.3.10.  Create index

To include the new project into the directory structure of PARTdataManager, you have to actualize the Index.

  1. Next mark the folder part.

  1. Then click on the button Update index. (The button is only active at top level.)

    --> The Update index window opens.

    After completed updating "Finished!" shows up.

    The new project has been integrated into the PARTdataManager directory.

  2. Save the file.

  3. Switch to project level.

    -> The Start PARTdataManager button becomes activated.

  4. Click on it.