For
the sake of the training and i order to not have to define all
variables that belong to the part, these are already located in a
file which will later be imported.
Define one variable as an example:
Click the
field Variables in the menu
field Variable.
Enter the Variable names.
Note
To keep equations concise, Variable names should
be preferably short. The
maximum length of a variable is
10
characters.
Umlauts (ö,ä,ü) and special
characters are not
to be used!
Capital letters
must be used. I.e., if you wrote a capital “L“ as well as a
small “l” within your variable templates, you have to
distinguish them as e.g. “L1“ and “L2“!