powered by CADENAS

Manual

Manual

8.3.4.1. Create geometry *.3db

  1. Click on “single_part-project.3db”. --> The Preview of the component geometry is displayed in the Edit project menu area. No drawing has yet been entered in this window.

  1. Click on the Edit button.

  1. Click on OK in the Edit file menu window. The Use variable from table option button is not yet relevant since no table from which you could use the variables yet exists .

--> PARTdesigner is launched.

  1. Create the Geometry/ *.3db file of your component. This is to be a cap nut in the example.

  1. Save the *.3db file and close PARTdesigner.

--> The geometry of the cap nut has now been included in PARTproject as “single_part-project.3db”. The preview shows the corresponding display.

--> Later, the geometry of the cap nut will be able to be seen as 3D preview in PARTdataManager Part view.