powered by CADENAS

Manual

Manual

13.5.1.7.1.6. Example 3

Excluding rules depending on availability of one and/or more other parts in an assembly:

The Hinge bearing bracket 180 Type K should exclude the Hinge bearing bracket 90 Type G in the assembly configuration.

Selected part is Hinge bearing bracket 180 Type K.

  1. Set a checkmark at Do not use the following rules if this one is used .

    --> The buttons Add and Delete are now active

  1. Click on

    Add.

    --> In the Rule browser window you can see the part overview of the assembly.

  1. In order to cancel the rule that connects Hinge bearing bracket 90... into the assembly, you must carry out the settings in the Rule browser.

Valid is:

Hinge bearing bracket 90 Type G cannot be part of the assembly as soon as Hinge bearing bracket 180 Type K is accepted into the configuration.