Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
4.3.3. Simulation -
Specification for Mechatronics Concept Designer (MCD)
4.3.3.2. Example for
a rotative simulation with an AFAG RE-50 rotary module
|
|
---|---|
Prev | Next |
Switch into the configuration mode in PARTdataManager and check which rule is the connection between the moveable parts – e.g. module and table. Open the rule then.
In the area Positioning, the checkbox Rotation „free“ must be activated and also Min. and Max. values must be specified according to the physical limits of the “real” product.
Click on Simulation, then Add, choose Actuator > Actuator Linear > Physical Limit (Rotation) and confirm with OK.
Determine the attribute values according to the real product.
Optionally, motion profiles can be set up. Compare above.
The part is ready for export and testing now. See below.