powered by CADENAS

Manual

Manual

11.5.3.2.  Copy

This command makes a copy of the currently marked table rows or cells. This copy can then be positioned in the table with Paste.

  1. Mark a table area.

  2. Click on the Copy command.

  1. "Skip" to the row above which the copy is to be inserted in the table.

  2. Click on the Pastecommand.

--> If you have marked only specific cells – not complete rows – a new row is created or new rows are created only with the marked contents of the original table.

In the example, the mouse cursor was in the first row when Insert was selected.

Consequently, the first row is moved down two rows by the two rows inserted.