powered by CADENAS

Manual

Manual

6.5.3.3.2.1. Changes at directory level

At directory level the menu item Set QA status has no sub-menu items.

Set QA status

Set QA status

Select the new QA status in the pull-down menu. It is possible that there is no selection available.

Dialog window set QA status

Dialog window set QA status

[Note] Note

The QA status provided depends on current status and the role assigned at login!

[Note] Note

It is impossible to set up a QA status of a superior directory, if a hierarchical subordinate project / directory has a lower QA status! (see error message below)

Set QA status - error message

Set QA status - error message

Using the option Set status in projects and directories a status can be set in projects and subdirectories. In this case you will not get an error message.

Using another option"Set only if the current status is", you can limit or specify the status allocation to your needs.

[Note] Note

The selection of a comment in the pull-down menu is obligatory! (See also Section 6.6, “History tab page”)

When selecting "Other" you can add any comment in the active text field.