powered by CADENAS

Manual

Manual

3.3.5.3.  Create preview images

Via Export files in batch run you can create preview images used within the program for the directory structure.

In Part selection a preview image is located for each catalog, directory and project level.

Preview images in the PARTdataManager

Preview images in the PARTdataManager

The preview image for the catalog can be created externally and then imported. See Section 4.7.2.1.14.3.1.3, “Alternative: Create preview images externally and then import ”.

For the preview images of parts, you also have an automatic variant available. Via the Export files in batch run command, the preview images can be created in the batch run. See Section 4.7.2.1.14.3.1.2, “Preferences”.

The function is available on project and directory level both in PARTdataManager [5], as well as in PARTproject:

  • Start in PARTdataManager

    PARTdataManager -> Export files in batch run

    PARTdataManager -> Export files in batch run

  • Start in PARTproject

    PARTproject -> Export files in batch run

    PARTproject -> Export files in batch run

    [Note] Note

    PARTdataManager must be installed.



[5] Only in Developer mode. Detailed information concerning the mode settings can be found under Section 1.1.6.6.2.3.1, “ Key "IsAdmin" - User mode ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.