powered by CADENAS

Manual

Manual

4.7.2.1.9.  Move folder

..."cuts" a directory/folder from its position in the tree. The directory or the folder can be "pasted" at a different position in the tree via Insert folder .

  1. Mark the directory or folder.

  2. Mark the destination directory and click on the Move foldercommand.

  1. Mark the destination directory and click on the Insert folder command.

    --> In the Move folder window you can see the source and target directories.[a]

[a] If one assumes that through moving the directory, all other directories (assemblies, whose properties refer to this directory) are affected, set a checkmark at Adapt links in assemblies and enter the Assemblies path (Browse ...). See Section 4.7.2.1.7, “ Rename folder ”.

  1. Confirm with OK.