powered by CADENAS

Manual

Manual

5.6.  Add projects to classification

A very important search and find option, aside from parts selection via the dialog page Catalogs is the dialog page Classes.

This chapter would like to assist you in classifying projects.

These could be:

  1. Your electronic CADENAS product catalog

  2. Via the CAD interface with the Own parts library function

    PARTsolutions  
    Insert 3D
    Replace
    Verify if up-to-date
    Execute Geometric Search
    Standard and supplier parts library
    Own parts library Insert
    Connections library Import entire directory
    Embed library into CAD user interface  
    Extras
    Settings
    About CADENAS PARTsolutions

  3. Via Classimporter, parts structured in catalog form

    (Detailed information about the Classimporter can be found under Section 2.1, “ Classimporter ” in PARTwarehouse Manual.)

A number of functionalities simplify the procedure.

Classifications can be conducted at the project and directory levels.

Additional functionalities are available to you at the directory level.

The following information is divided into 4 main parts:

  • Allocation at project level

  • Allocation at directory level

  • Index update

    [Note] Note

    After changes, in PARTadmin -> Index administration, the search index must be updated so that new allocations can be displayed in the PARTdataManager.

    The update has to be performed both for concerned projects and for the classification!

  • PARTdataManager

    Read here on how to use class information in the PARTdataManager.

[Note] Note

All classification and attribute informations are transferred to the interface, in other words the CAD, upon export.