powered by CADENAS

Manual

Manual

9.3.2. Template

In the following you will see an example how you can work with templates in the PARTdataManager.

[Note] Note

You can follow the example once you have installed the training.cip.

(Training/assembly/hinge/bsp- hinge)

In contrast to the configuration, the template assembly (file format *.sbl)completely, or at least, partially, has an automatic generation.

In the Assembly the Start element and the connecting assembly parts (see Fig. „Templates with complete self-assembly“) show up immediately.

The selection list area remains empty.

Template types

  1. Templates with complete self-assembly are able to configure themselves 100% alone.

    There are no longer any free (green) connection points. All connection points are displayed in black lettering.

    Single elements can be removed, or (if available) replaced by alternative characteristics

    After a row change, the template reassembles itself completely.

    Templates with complete self-assembly

    Templates with complete self-assembly

  2. Templates with partial self-assembly have a certain basic structure with which the generate themselves. Some Connection points are still open (green) and may be occupied by pre-generated elements. This template variant shows a mix between configuration and full template. It may be changed and/or reduced.

    [Note] Note

    The example can be found in the trainings catalog under "Bausteine/Bausteine Auto".

    Template with partial self-assembly (configurable further)

    Template with partial self-assembly (configurable further)

  3. Fixed template: It assembles itself 100% alone, however -in contrast to other template types - it can neither be changed nor reduced.

    [Note] Note

    As user you do not have the opportunity to remove the fixation.