powered by CADENAS

Manual

Manual

6.7. QA check tab page

After a directory / project has passed quality checks by the editor and achieved a status of 4, the editor starts Test project in the context menu of the directory tree.

Testing a project

Testing a project

After an erroneous pass the directory / project is automatically set back to status 3.

Didn't pass the test

Didn't pass the test

Passed the test

Passed the test

After a passed test, the project automatically achieves QA level 5.

Any error messages emerging at automatic QA check are recorded during the testing in the dialog window QA check.

Dialog window - QA check

Dialog window - QA check

Furthermore any error messages are listed at the dialog page QA check and stored until trouble shooting.

Both dialogs are identical in principle.

Dialog window - QA check

Dialog window - QA check

By Marking an error line, the text is displayed in the text field below. This can be helpful if a text passage is too long for getting displayed in the error line.

Using the Context menu at error line you are directly able to call up the suitable program for error analysis and correction.