Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following is true in general for using the buttons:
Activate button with simple mouse-click. -> The function of the button is then attached to the cursor.
Move the cursor to the desired spot within the sketch. -> Depending on the function of the button, the snap (circle symbol) will become visible.
Carry out the function of the button at the desired spot with a simple mouse-click (for example, "insert line", etc.).
In the New 2D drawing mode, aside from the Sketcher mode, you also have the following toolbars available:[42]
The following sections explain the individual buttons of these toolbars.
In the Text position field you can determine the direction of the text to the set position X/Y ( red point at the A symbol). |
The Change parameter window opens. Here you may adjust the Scale factor and determine the Reference point. |
|
Ellipse by point on main axis and hull edge point : In the Change parameter window you can adjust the coordinates through values and/or variables. |
Ellipse by point on main axis, width and height : See Ellipse by point on main axis and hull edge point. In the Change parameter window you can regulate the dimension of the ellipse via Width and Height (see figure at right). |
Ellipse by main axis angle, width and height : See Ellipse by point on main axis and hull edge point In the Change parameter window you can regulate the dimension of the ellipse via width, height and the angle between the x and main axis (see figure at right). |
See Ellipse by point on main axis and hull edge point, then: -> The segment, which can be found in clockwise direction between a) and b, remains intact! Start and End point can be adjusted in the Change parameter window. |
Ellipse segment by point on main axis, width, height, start- and end point : See Ellipse segment by point on main axis, start- and end point. Width and Height can also be adjusted in the Change parameter window. |
Ellipse segment by point on main axis, width, height, start- and end angle : See Ellipse segment by point on main axis, start- and end point. Start and End angle refer to the main axis. Both can be adjusted in the Change parameter window. |
Ellipse segment by main axis angle, width, height, start- and end angle : See Ellipse segment by point on main axis, start- and end point. In the Change parameter window you can additionally determine the dimension of the ellipse via the angle between the x and main axis. |
The dimensioning mode can be called up via:
Call up the Dimensioning mode via respective toolbar button or context menu command.
|
Radial with angle and distance: The angle (concerning the x-axis) of the dimensioning can also be adjusted in the Change parameter window. |
|
Note | |
---|---|
Rotationally symmetrical points are dimensioned from point to line with help of the half value function. Though the depicted dimension line only describes half of the dimensional length (therefore "Half value"), the dimensional value, however the whole dimensional length! |