powered by CADENAS

Manual

Manual

6.5.3.2.2. Level 2

Coming from level 2, the following QA levels can be set:

Set QA status

1 - Not released yet

3 - In progress

Customer himself is setting status back to level 1, because relevant data is missing or incorrect.

The Editor has two possibilities:

  1. He sets the status up to 3, because he is starting work

  2. He sets the status back to 1, because data is incomplete, unsuitable or incorrect.

    Now it is the customer's turn again.

    [Note] Note

    All QA status changes must be commented on.

    Comments can be viewed at any time on the dialog page History.

    See Section 6.6, “History tab page”.