powered by CADENAS

Manual

Manual

4.8.3.3.  Variants

The dialog area Variants is optional.

If you do not want the same Dimensioning views or 3D models to be used for all component attributes, you can define variants at this point. This means that you assign specific views and/or models to the various attributes via variable values.

Example: If the variable DG has the value 10, then din_1587-seitenansicht.pra and din_1587-draufsicht.pra are considered to be the dimensioning views and din_1587-nenngewinde.3gb and din_1587-kernloch.3db are considered to be the 3D models.

Dimensioning views: enter the dimensioning view(s) relating to the relevant variant at this point.

3D models: enter the 3D model(s) relating to the relevant variant at this point.