powered by CADENAS

Manual

Manual

9.5.1.7.1.1. Properties
  • Name: ...of the rule.

[Note] Note

The name of the rule has to be unique!

  • Selection field:

Selection

Function

Forbid autom. build (X)

...excludes the part which is created by this rule from the automatic assembly build [a] through the user.

Admit autom. build (U)

...includes the part (which is created by this rule) in the automatic assembly build (by user).

Always build automatically (V)

...includes the part (which is created by this rule) in the automatic assembly build.

[a] Information to automatic assembly build in PARTdataManager is found under Section 3.1.3.1.5.4, “ Connect assemblies automatically ” in PARTsolutions / PARTcommunity4Enterprise - User manual.

[Note] Note

The abbreviation in parentheses in the configurator area indicate the used setting in the list field under Properties.

  • Exclusive : If there are different parts assigned to one connection point you can define a certain part as „exclusive“. Consequence: As soon as this certain part is selected the others (alternatives) are not available anymore.