powered by CADENAS

Manual

Manual

5.4.4.4.1. Element_<title_value>

The element is declared with "ELEMENT_" followed by a unique description for the element, which is declared in block "ELEMENT_grid" key "title".

Via the following keys, the display of the title is specified.

  • type = text

    Declares the element type and is mandatory.

  • parent

    It is mandatory that texts are placed in a frame element.

  • text

    Text of title

    Default: "Normalprojection"

    Variables (z.B. $NT.) are allowed.

  • Position and dimensions of text box:

    The following information is required.

    • position_x: indicates x-coordinates of box.

    • position_y: indicates y-coordinates of box.

    • position_w: indicates width of box.

    • position_h: indicates height of box.

  • text_size

    Indicates size of text. The minimal text size is '1'.

  • width_factor

    Indicates the stretch factor for the width of the text. The minimum possible value is '0.5'.

  • sizeable

    Indicates whether or not the size/position of the text element can be changed in Edit mode.

    Value range: true | false

  • translateable

    Indicates whether the text given under "text" is to be translated.

    A *.def file must be assigned here in which the translations for the texts are entered. Compare also Section 5.4.4.11, “ Translations ”.

    The def file must be entered in the frame element. Compare Section 5.4.4.9, “[ELEMENT_frame] Combine more elements in frame ”.

  • Use ratio specification

    use_ratio

    Value range: true | false

  • Rotation of title

    rotation

    Value range: horizontal | vertical

    [Note] Note

    For "vertical" the position specifications must be adjusted accordingly.

  • Direction of title

    text_align

    Value range: left (alternatively no specification) center | right