powered by CADENAS

Manual

Manual

5.4.1.6.1.  Mandatory parameters

Each part-notation must contain the following parameters:

  • ID

    The ID is automatically set.

  • Type

    When creating a new dimensioning at first a selection dialog box for the type definition appears. The type is displayed here.

    If it makes sense you may change the type via list field.

    [Note] Note

    The parameter fields are not updated until you have clicked Save changes .

  • Views

    At the desired 2D views, where the dimensioning shall be displayed, activate the checkbox.

  • Connection point

    The respective position number is placed close to the desired connection point.