powered by CADENAS

Manual

Manual

3.3.2.3.1.1. Defining variable names

For the sake of the training and i order to not have to define all variables that belong to the part, these are already located in a file which will later be imported.

Define one variable as an example:

  1. Click the field Variables in the menu field Variable.

  2. Enter the Variable names.

[Note] Note
  • To keep equations concise, Variable names should be preferably short. The maximum length of a variable is 10 characters.

  • Umlauts (ö,ä,ü) and special characters are not to be used!

  • Capital letters must be used. I.e., if you wrote a capital “L“ as well as a small “l” within your variable templates, you have to distinguish them as e.g. “L1“ and “L2“!