powered by CADENAS

Manual

Manual

9.5.1.7.1.4. Example 1

Dependence on a single condition:

The selected parts should only be connected if the variable value of the part AUGE is larger than 1.

  1. At Only use if set the checkmark.

  2. Right-click into the input area in order to open the corresponding context menu.

  3. Click on Choose variable....

  4. In the Variable browser set the condition AUGE@B>1 and confirm with OK.